Search Knowledge Base by Keyword
- Are iglidur materials resistant to my cleaning agent or special chemicals?
- Are iglidur plain bearings suitable for use in the food area?
- Are there antibacterial iglidur materials?
- Are there antistatic, electrically conductive or surge-arresting plain bearings?
- Are there iglidur materials made of renewable raw materials?
- Are there iglidur PRT slewing rings with a locking function?
- Are there iglidur PRT slewing rings with gears?
- Are there materials for use in drinking water?
-
Energy supply for robots
- Are e-chains compatible with Industry 4.0?
- Are igus e-ketten maintenance-free?
- Are plastic energy chains resistant to hot chips?
- Are plastic energy chains resistant to special chemicals?
- Are there any energy supply system for cleanroom class 1 and 2?
- Are there energy chains with FDA approval?
- Are there special energy chains with "Hygienic Design"?
- Can I also get a coloured energy chain?
-
Ethernet
- Are there halogen-free PVC cables?
- Can I harness an FOC cable in the field myself?
- Do cables become longer in hanging applications?
- How can I protect my cables/hoses (possibly multi-core cables) against damage?
- How does the capacitance of a drive cable become noticeable in practice?
- How does the capacitance of a drive cable become noticeable in practice?
- How is the right strain relief for cables to be selected?
- Is it permissible to operate the cable with the test voltage?
-
Linear guides
- Are lightweight linear guides the future?
- Are linear guides easy to install?
- Are linear guides ergonomic?
- Bearing change on the rail in 30 seconds
- Building linear carriages oneself, is that possible?
- Can I monitor the wear of my bearing systems?
- Corrosion protection of linear guides?
- Grease linear bearings? No thank you!
-
Liner
-
Motor control
- Can I also install the D3 DC motor control on a top-hat (DIN) rail?
- Can I connect an external switch to the D3 DC motor control?
- Can I set different acceleration profiles in the D3 DC motor control?
- CanOpen and the fast connection to the D1 motor control
- Do not take it too seriously. The D3 DC motor control in alternative use.
- How are the digital outputs of the d1 motor control connected?
- How do I connect a cable to the D1 motor control?
- How do I connect a DC motor control with a linear axis?
-
e-motors
- Articles coming soon
- Can I also install the D3 DC motor control on a top-hat (DIN) rail?
- Can I connect an external switch to the D3 DC motor control?
- How do I connect a DC motor control with a linear axis?
- How do I connect a proximity switch to a D3 DC motor control?
- Linear guides with detent
- What all can I adjust directly on the D3 DC motor control?
- Where do I use a motor control for DC motors?
- Which DC motors can be connected to the D3 DC motor control?
- How are installation sizes of ball bearings standardised?
- How much load can a ball bearing absorb?
- Metal, plastic, ceramics - when to use which ball bearing?
- Should ball bearings be greased?
- What are ball bearings for?
- What must be borne in mind when igus® ball bearings are installed and measured?
- When should I use a plain bearing – when a rolling bearing?
- Which ball bearings are suitable for electroplating equipment?
-
Ready-to-connect cables
-
Plug-in connectors
-
Ready-to-connect energy supply systems
- Avoidance of tolerances in design & orientation in 3D printing
- Dimensional deviations in the various 3D printing processes
- How accurately can a 3D printer print?
- How does a 3D printer work?
- How does a gear work?
- How expensive is a 3D printer?
- How long does a 3D printing component last?
- How much does 3D printing cost?
- Are e-chains compatible with Industry 4.0?
- Can I monitor the condition of energy chains on the computer?
- Can I monitor the wear of my bearing systems?
- Do I have to buy a computer to monitor the system?
- Do I need Internet for monitoring my equipment?
- Do we have to let igus on our corporate network?
- How are intelligent insights gained from pure sensor data for Smart Maintenance?
- How does the maintenance system know that a component should be replaced?
- What are the available soldering methods?
- What is electrical resistance soldering?
- What is flame soldering and what are its advantages?
- What is furnace brazing and what are its advantages?
- What is hand soldering and what are the advantages?
- What is induction brazing and what are its advantages?
- What is reflow soldering?