Are e-chains compatible with Industry 4.0? - igus Blog

Are e-chains compatible with Industry 4.0?

Marco Thull | 4. July 2019

Are e-chains compatible with Industry 4.0?

You are here:

In order to digitise processes, more users are integrating machines and systems into the Internet of Things. This benefits, for example, the maintenance. So far, service technicians had to regularly inspect thousands of components on site. A job that is not only time-consuming, but also error-prone. Small defects are easily overlooked. The alternative in the Industry 4.0 era: Networked sensors that continuously transmit the condition of components to a computer.

smart plastics in use at an Austrian automotive supplier

e-chains from igus are ready for the digitisation era. Among other things, the company has developed a break detection system called EC.B. It consists of a polymer wire running inside the e-chain and the online module ICOM. If damaged, the system alerts the user. This then performs a proactive maintenance – before it comes to a system failure.

You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!