What shafts should I use for iglidur plain bearings? – igus Blog

What shafts should I use for iglidur plain bearings?

Lars Butenschön | 9. July 2019

What shafts should I use for iglidur plain bearings?

You are here:

For almost every shaft, there are appropriate iglidur materials that are highly wear-resistant, which means they have a long service life – whether the material is aluminium, hardened steel or carbon fibre compound. You can find the best combination in comfort with the help of the iglidur Expert system. The surface of the shaft should not be too smooth. We recommend a roughness of Ra 0.2 to 0.4 µm. The ideal tolerance for the outer diameter of the shaft is h9.

You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

Plain bearings

Newsletter:

Choose a topic now