The global circular economy is shrinking. It is high time to act. One solution would be to recycle technical plastics, but that has so far been quite cumbersome. We will show you how plastic recycling is finally becoming easy.
In today’s increasingly globalised world, service is often a nuisance for everyone. You have a problem with a household appliance, perhaps an oven, and you have specifically chosen a German brand. Luckily, the instructions also include a flyer with service numbers for each country. But when you enter the number into your phone, you always […]
One day after the trade show It happened near the beginning of the Hannover Messe, not all that long ago. They say that sometimes the best ideas come from a mix of nonsense and a little alcohol. Something like that must have been in play when the idea for the TRX emerged. Two exhausted, thirsty […]
Today I would like to introduce a topic that is often overlooked or not taken seriously, but can have a significant impact on the success of your business: professional energy chain installation. Whether you run a small manufacturing operation or manage a medium-sized facility, investing in the right expertise for your energy chain systems can […]
I would say that they are not. Metallic plain bearings with relatively thick walls (conforming to DIN 1850, for instance) are used in many heavy-duty applications in agricultural engineering and construction machinery. Typical bearings are steel bushings and plain bearings made of non-ferrous metals (bronze = copper + tin, brass = copper + zinc), but […]
Cables are used in many areas. Some cables must meet very special requirements or withstand certain external factors. Consider cables that are used under water. What problems arise for cables used in underwater applications? What solution approaches are there? Longitudinal and transverse waterproofness There are a number of things that cables that are used under […]
Die zwei häufigsten Gründe für die Fertigung von Antriebs- und Gewindemuttern mittels 3D-Druck Verfahren sind der Bau von funktionalen Prototypen und die Herstellung von komplexen Sondermuttern. In der Produktentwicklung werden mitunter mehrere Modelle konstruiert und getestet – mit dem Rapid Prototyping Verfahren kann die Herstellung von seriennahen Varianten und Anpassungen sehr schnell erfolgen, was einen […]
igus motion plastics – tribologically optimised high-performance polymers for moving applications – are the result of decades of research and development work. Each igus material, known under the iglidur brand name (https://www.igus.eu/iglidur), is thoroughly tested in our 3,800m² test laboratory. We have a huge material selection and are constantly adding new materials developed for various […]