The global circular economy is shrinking. It is high time to act. One solution would be to recycle technical plastics, but that has so far been quite cumbersome. We will show you how plastic recycling is finally becoming easy.
In today’s increasingly globalised world, service is often a nuisance for everyone. You have a problem with a household appliance, perhaps an oven, and you have specifically chosen a German brand. Luckily, the instructions also include a flyer with service numbers for each country. But when you enter the number into your phone, you always […]
One day after the trade show It happened near the beginning of the Hannover Messe, not all that long ago. They say that sometimes the best ideas come from a mix of nonsense and a little alcohol. Something like that must have been in play when the idea for the TRX emerged. Two exhausted, thirsty […]
Today I would like to introduce a topic that is often overlooked or not taken seriously, but can have a significant impact on the success of your business: professional energy chain installation. Whether you run a small manufacturing operation or manage a medium-sized facility, investing in the right expertise for your energy chain systems can […]
The new igus P41.80RI roller chain with integrated iglidur plain bearings has been doing its job on the gigantic ship unloader cranes from EMO B.V. in Rotterdam since the end of 2015. EMO B.V. is one of the largest bulk terminals in Western Europe. With a trolley travel of over 100 m, a travel speed of up to 4 m/sec and an additional load of over 50 kg/m, it is one of the most demanding energy chain applications in the port crane sector.
The e-spool is a chain-based drum application without a slip ring. Ideal for applications and lifting devices that have no space for a collection basket (lift band). The cables routed in the chain are not exposed to tensile stress, which has a positive effect on the service life of the cables.
Linear axes and linear modules can be driven differently. Which system is the right one for me – lead screw drive or toothed belt drive?
A decisive point for the smooth application of the beer lift is the use of the correct high-helix thread system. The length of the lead screw is approx. 1 metre. In order to be able to guarantee the service life as long as possible, there are two important points to consider.