Our E4.350 energy chain from the E4.1 series is the world’s largest polymer energy chain and has been in operation in Antwerp for over 10 years on a travel
…
…print bed, upload the 3D model and you’re done. The installation and set-up costs are low. But the run time per part is long, resulting in a relatively high part…
…polymer slewing ring ball bearings with stainless steel balls. The special feature of the bearing rings is the wear-resistant ball bearing material. The slewing ring ball bearing is 100% lubrication-free,…
…cover many cables for industrial use. Other strands are installed there, which the user often does not know. Out of ignorance the user connects them and brings together two high-quality…
…Products such as plain bearings, linear guides and energy chains made of high-performance igus polymers have been used in various areas of medical technology. Lubrication-free, cleanroom compatible, media-resistant, corrosion-free, quiet…