For pivoting and rotary movements of up to 270°, it is important that cables and hoses are laid in the energy chain’s neutral phase. Why is this so important?
…
…article number for the energy chain you want. An example would be 2500.05.075.0. NC.
What if there are transverse forces?
If the energy chain is installed on a carriage…
…dirt (e.g. very advantageous in exterior areas) Lubrication-free (e.g. no disturbing grease in the interior) Tested in the igus laboratory: https://www.igus.co.uk/info/linear-guides-test-wear-dryspin Find all available materials and lead screws in our…
…it is essential that all components, from steel structures up to the energy chain and their cables, are designed and approved accordingly. To ensure a high availability of the system…
…17dB(A) quieter: optional noise dampening can be retrofitted as an accessory component at any time Order a free E4Q energy chain sample here Vote Up +0 Vote Down -0You already voted!…