…the plain bearings? ← All Topics
iglidur plain bearings are held in place in the smaller housing hole by means of the press-fit. Certain parameters such as high or especially
…
…is therefore a difficult undertaking and is only on the agenda at longer intervals – and this is where xiros polymer ball bearings from igus play a role in the…
…devices or camera and sensors. Discover the stop-motion series, which has these characteristics and for which you can determine the displacement forces yourself:
Vote Up +3 Vote Down…
The high speeds of the robolink joint are tested with this testing system. The four degrees of freedom of the double joint are accelerated to an angular velocity of
…
…For higher temperatures, people refer to the process as high-temperature soldering or even welding. While with soldering, only the solder is melted to connect parts; with welding, the metals that…