…fixed and these of course comply with chainflex cables.
The risk analysis
“Necessary risk analysis according to the machine directive, because unknown components (cables) are inserted. “
”…
…etc. is very high, the customer is usually advised not to do this. Apart from this, expensive special tools and specialist knowledge are needed for harnessing. In the case of…
…the cables during operation using high-frequency technology. The output takes place both in the i.Cee dashboard and directly via a coloured alarm message:
LED (lit)DescriptionGreen+ LED button Device is working…
…are wound in short pitch lengths around a centre element of high tensile strength. The forces and effects described above are thus compensated for.
Vote Up +0 Vote Down -0You…
…indicates how high the impedance is that a signal has to overcome when it is propagated in a cable.
Vote Up +0 Vote Down -0You already voted! Tags: Wave impedance…