…which can show off their maintenance-free dry-operating properties and high mechanical strength in construction machinery and commercial vehicles.
Since different pairs of plain bearings and bolts can differ…
…produce the ball bearing rings by injection moulding . This offers users the following advantages:
High wear resistance due to the shape under high pressure Homogeneous material distribution Cost-effective production meaning economical…
…maximum pv value is usually indicated. This is the amount of heat that can be removed per time unit due to the heat dissipation capacity of the materials involved. If…
…mm the linear travel per revolution of the lead screw. In contrast to a metric or a trapezoidal lead screw, the high helix lead screw has a high pitch….
…with high loads, high temperatures or in heavily polluted environments, a standard lead screw nut should always be used. The reason for this is that all three principles are cancelled…