…industry shows the economic potential of this technology: For an energy chain, the manufacturer predicts the expected service life under specified conditions of use. Sensors in the energy chain send…
…go wrong here. Especially when the cable concerned is used for dynamic applications in energy chains, incorrect unreeling can have fatal consequences. To be honest, when I was in my…
Flame soldering is a thermal joining process for metallic materials that are connected with a solder during this method. The thermal energy required for this procedure
…
…of lubrication and the coefficient of friction should also be taken into account. But why are these values so important?
Piston rings that are exposed to high pressure…
…ring => low cost solution).
# worm shaft made of hard anodized aluminum, or as injection moulded plastic part (iglidur RN33), additional materials as an Option.
# axial bearings…