Drive technology - igus Blog - Page 2 Drive technology - igus Blog - Page 2

Category:

Drive technology

How to connect igus® encoders with Beckhoff and B&R

Adriana Glazer | 7. April 2021

There are control systems whose encoder card is usually compatible with 24V and/or single-ended encoders. igus motors, however, work with 5V and as line drivers. A connection of these two voltages requires another component or a special encoder card.Today we are looking at the connection of igus motors to control systems that work with 24V […]

Read more...

Construction and assembly of lead screw motors – the basics

Adriana Glazer | 20. November 2020

As a well-known manufacturer of engineering plastics, igus has meanwhile established itself in the minds of the engineering universe. But around these core products a huge product world has developed with over 10,000,XXX different products. One of them is the lead screw motor. As the name suggests, a lead screw motor consists of a lead […]

Read more...

Thread direction

Zoe Moser | 9. October 2020

What is the difference between left-hand and right-hand threads? How can I recognise the thread direction even without a test? The thread rotation direction right or left can be easily determined with a visual inspection. If you look at the lead screw from the front, you can best see the difference between left-hand and right-hand threads.

Read more...

Bearing replacement for linear axes with toothed belt drive

Thomas Urbach | 30. September 2020

The bearing replacement for linear axes with belt drive is usually very time-consuming and complex. But it is easier, faster and cost-effective. How to find out here in this blog.

Read more...

motor alignment blog

Motor alignment on igus axis – this is how assembly works

Adriana Glazer | 29. September 2020

Anyone who has ever wanted to order an igus linear axis is inevitably asked at some point what orientation the motor should have. Left, centre, right, 0° or 90°? It all sounds like choosing your party before the local elections, but it is much easier than that. What is meant by motor alignment? By motor […]

Read more...