All messages - igus Blog - Page 61 All messages - igus Blog - Page 61

New ball bearing material – ideal for applications in the semiconductor industry

Patrick Czaja | 19. May 2022

The semiconductor industry always has demanding application environments. For example, installed components must always run flawlessly in order to keep plant productivity rates high. The etching of printed circuit boards or the production of LCD displays are two examples to illustrate this.

Read more...

Remote condition monitoring of energy chains??? This little wonder box makes it possible: the SMS module

Richard Habering | 18. May 2022

Internet of Things, big data and autonomous robots: the transition to Industry 4.0 is in full swing. This also applies to components that work in machines and have long since become smart by providing data on their condition, for example. But integrating smart technologies is often complex for companies and involves external installation effort. This is exactly where we start with the SMS module for our i.Sense systems.

Read more...

The autoglide 5 lasts longer than you think …

Christian Strauch | 16. May 2022

One might think that I would have said everything you could say about the autoglide 5 by now, but I haven’t come close. The autoglide 5 still has some advantages over the basic chain, including the following: The autoglide 5’s special crossbars increase the load-bearing surfaces or sliding surfaces. Larger sliding surfaces also mean lower […]

Read more...

New ball bearing material for medical technology applications – xirodur® MT180

Patrick Czaja | 9. May 2022

An innovation has been added to the range of xirodur materials. The xirodur MT180 material complies with DIN EN ISO 10993, and individual components are certified as USP Class VI. This allows safe use in medical technology applications.

Read more...

Flanged bearing – what you need to think about

Lars Butenschön | 6. May 2022

In order to fix plain bearings in the receiving bore so that they are form-fitting, a collar or flange is attached on one side or, in some designs, both sides. If you use flanged bushings in your application, some design considerations will help avoid bearing damage. The housing hole The housing hole should be perpendicular […]

Read more...