Plastic ball bearings - igus Blog Plastic ball bearings - igus Blog

Keyword:

Plastic ball bearings

Kugellager in Pumpen

Ball bearings in pumps: prevent machine failures with polymer

Patrick Czaja | 4. February 2021

Pumps and compressors are used in a wide variety of industries. Whether, for example, hose pumps in medical and food technology or water pumps in pool technology: just as the heart is for humans, these types of pumps in industry are also to be regarded as the heart of the system.

Read more...

Ball bearings in semiconductor technology: why you should rely on igus®

Patrick Czaja | 21. January 2021

Semiconductor manufacturers face some challenges in the industry. Because they are always striving to achieve high productivity rates in their systems. Stringent and, above all, demanding application environments are commonplace in semiconductor technology, so components integrated into the process must function smoothly. In the etching of printed circuit boards or the production of LCD displays, […]

Read more...

Ball bearings in the household: the invisible facilitators

igu-blog-adm | 19. January 2021

Ball bearings are our daily bread. As abstruse as this may sound at first, this sentence says how important ball bearings are in our world. Because wherever parts turn, move or rotate, ball bearings, usually also referred to as roller bearings, are used. Without them, the world would literally stand still. Ball bearings are commonplace […]

Read more...

Why your ticket machine ball bearings should be from igus®

Patrick Czaja | 7. January 2021

Ball bearings in ticket machines where requirements for installed components are stringent. igus polymer ball bearings are expanding their advantage over metal ball bearings in this segment. They are not only maintenance-free and lubrication-free – they also ensure that the application environment is free of contamination. Searching for contamination of tickets and banknotes: not here

Read more...

Ball bearings in material handling: why igus® ball bearings are the ones to beat

Patrick Czaja | 5. January 2021

There are two decisive arguments for efficient material handling: freedom from lubrication and freedom from maintenance. Ball bearing reliability and load capacity in material handling are also necessary to ensure smooth running.

Read more...