Plastic ball bearing xiros®
The semiconductor industry always has demanding application environments. For example, installed components must always run flawlessly in order to keep plant productivity rates high. The etching of printed circuit boards or the production of LCD displays are two examples to illustrate this.
Night vision devices are mostly associated with types of binoculars that enable as well as enhance visual perception in the dark. They are used by the military or police, security services, but especially by hunters or naturalists. It doesn’t always have to be the familiar binocular shape. Developers always adapt to the different environments so […]
If the metal ball bearing is a fixed or floating bearing, the outer and/or inner ring are firmly connected to the shaft or housing. The easiest way to mount this type of bearing is to press it into place. However, certain tolerances are necessary in the dimensions for the shaft and housing. In general, it […]
Germany has been one of the largest industrial nations and technology leaders for many decades. To ensure that this remains the case for many generations to come, universities and colleges are important institutions where thousands of students and researchers rack their brains over new technologies every day. We are very happy to support students through […]
Self-aligning ball bearings (DIN 630) are double-row rolling bearings, consisting of an inner ring with a common ball raceway and an outer ring characterised by a hollow spherical design. Due to the hollow shape of the outer ring and the resulting angular mobility, self-aligning ball bearings are used in applications with larger misalignments, shaft deflections […]