Indoor crane
For many lifting applications, a compact and space-saving solution is extremely important. However, the more cables have to be routed together in a system and the longer the lifting height, the less the choice of possible solutions. When the already presented liftband or e-spool reach their technical limits, the only thing left is the so-called zig-zag installation method.
A wide variety of cables are used in modern crane systems. The load due to constant movement is the same for all trolley and crane supply cables.
Mobile energy, control and data supply to equipment requires a very complex system. For the overall system to perform its function, the individual system components must be harmonised.
For many lifting applications, a compact, space-saving solution is extremely important. But the more cables coming together in a system and the higher the stroke, the fewer the plausible solutions. If the liftband or the e-spool reaches its limits, the zig-zag installation is often the only thing that remains.
The e-spool is a chain-based drum application without sliding contacts. Ideal for applications and load-carrying equipment constructions that have no room for a collection basket (lift strap). The cables guided in the chain are not exposed to tensile strain, which has a positive effect on the service life of the cables.