…These include iglidurX, iglidur H1 and UW500. In our plain bearings shop and with the iglidur Expert system, these properties can be used for filtering.
Underwater view of the sea…
…What is the difference between iglidur materials and simple plastics such as POM and PA6? ← All Topics
iglidur materials are so-called compounds, plastics that have been mixed with special
…
…What is the difference between iglidur materials and simple plastics such as POM or PA6? ← All Topics
iglidur materials are so-called compounds. Compounds are plastics to which special
…
…aircraft environment.
In order to prove the resistance of four selected iglidur® materials against Skydrol LD-4, we carried out some tests.
Test set up
Three test specimens made…
…manufactured, the tools may need to be cleaned with corrosive chemicals, washed with high-pressure steam or disinfected with high-intensity ultraviolet light or radiation.
Ordering FDA parts such as linear…