…Weight saving compared to metal bearings Maintenance-free, without liquid/lubrication Disadvantages: Selection can sometimes be difficult Less suitable for very high loads beyond 80-100MPa surface pressure Combination of high loads and…
…energy chain with crossbars every link unsupported length identical to that of an energy chain with crossbars every link
In these energy chains crossbars are installed in every chain
…
What is the maximum possible travel length? Created On1. July 2019 byMarco Thull Print You are here: Main Energy chains What is the maximum possible travel length? ← All Topics…
…of the P4 chain series is the heavy duty version, P4.HD. It is not just a P4.1 with wider side links. With the P4.HD a new chain link design has…
…are always in a position to equip your energy supply system with intelligent sensors at the next maintenance appointment without a long lead time.
The smart plastics complete…