…if there is not enough space, or the requirements for movements are very high? This is exactly where igus introduces the high-end TPE cables. In addition to the PVC and…
…classic recycling, materials are sorted by type and broken down into their constituent components, which serve as raw materials. A PET bottle becomes a new bottle or a sports shirt….
…to coolants, reduce vibrations and can replace expensive materials.
Additional links:
Application example: https://www.igus.eu/info/plain-bearings-machine-tools-manufacturing?L=en
Further information on plain bearings: https://blog.igus.eu/die-3-groessten-irrtuemer-ueber-kunststoff-gleitlager/
Vote Up +0 Vote Down -1You…
…HACCP recommended?
All companies in the food industry are obliged to carry out their own checks according to HACCP. This includes operators of vending machines in which open foodstuffs…
…deliveries The sliding principle and the use of innovative materials
From time savings, reduced maintenance and weight savings up to noise level reduction. The advantages of a linear plain
…