How are bearings changed in the case of a low-profile guide system? - igus Blog How are bearings changed in the case of a low-profile guide system? - igus Blog

How are bearings changed in the case of a low-profile guide system?

Michael Hornung | 30. June 2019

How are bearings changed in the case of a low-profile guide system?

You are here:

The drylin N low-profile guide system consists of an anodised C-profile in which a sliding carriage travels. The basic carriage is a zinc die-cast component and is clipped into a sliding frame made of iglidur J polymer. Completely dry, clean and quiet when sliding.

The two halves of the sliding frame can be ordered at a later date after the carriage. Simply pull the carriage out of the rail, clip into the new frame and that’s it. Rail and basic carriage can easily be re-used.

This is how it is done:

You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

Bearing change Linear technology

Newsletter:

Choose a topic now