Plain Bearings - igus Blog - Page 5 Plain Bearings - igus Blog - Page 5

Category:

Plain Bearings

Uwe Sund

Interview: how to avoid complaints due to lack of lubrication

Marc Preinesberger | 15. July 2022

As an industry expert and product manager for heavy-duty plain bearings at igus GmbH, Uwe Sund encounters these challenges every day in his work with manufacturers of machines and vehicles for agriculture, construction and forestry. In the interview, he explains how manufacturers can prevent complaints due to insufficient lubrication.

Read more...

Which ball bearing is suitable for high speeds?

Patrick Czaja | 2. June 2022

Deep groove ball bearings according to DIN 625 standard are the most commonly used ball bearings in industry. Depending on the application, plant operators have different requirements for the installed machine components. For deep groove ball bearings, for example, the possible speeds per minute are usually important. Which ball bearing is suitable for high speeds? And that even made of plastic? xiros is the answer.

Read more...

New ball bearing material – ideal for applications in the semiconductor industry

Patrick Czaja | 19. May 2022

The semiconductor industry always has demanding application environments. For example, installed components must always run flawlessly in order to keep plant productivity rates high. The etching of printed circuit boards or the production of LCD displays are two examples to illustrate this.

Read more...

New ball bearing material for medical technology applications – xirodur® MT180

Patrick Czaja | 9. May 2022

An innovation has been added to the range of xirodur materials. The xirodur MT180 material complies with DIN EN ISO 10993, and individual components are certified as USP Class VI. This allows safe use in medical technology applications.

Read more...

Flanged bearing – what you need to think about

Lars Butenschön | 6. May 2022

In order to fix plain bearings in the receiving bore so that they are form-fitting, a collar or flange is attached on one side or, in some designs, both sides. If you use flanged bushings in your application, some design considerations will help avoid bearing damage. The housing hole The housing hole should be perpendicular […]

Read more...