Plain Bearings
I would say that they are not. Metallic plain bearings with relatively thick walls (conforming to DIN 1850, for instance) are used in many heavy-duty applications in agricultural engineering and construction machinery. Typical bearings are steel bushings and plain bearings made of non-ferrous metals (bronze = copper + tin, brass = copper + zinc), but […]
The concern is often optimisation of component or system service life. In the packaging and beverage industries, machines operate at especially high frequencies, and component service life plays an important role. But it can be just as important to extend the product service life or life cycle. Or protect the product from damage. There are […]
As the name suggests, the original purpose of this material is to be used as a machine element in piston engines. I especially associate “piston rods” with their use in hydraulic cylinders and have a hard chrome shaft in mind. Generally, this is not a valid statement. For various reasons, nitride shafts are now also […]
The modern car interior has many different knobs, dials and switches. Whether it is the adjustment of the window, air conditioning or sound level – we are increasingly resorting to the cleverly placed rotary adjusters in the interior. All these controls are directly related to the quality perception of the vehicle and can influence a possible car purchase.
In the water bath the extrudate is guided by rollers and kept at a distance. The rollers run with pressed-in stainless steel ball bearings without seals. These run completely under water. Despite the stainless steel design, these had to be replaced at regular intervals due to corrosion. igus polymer ball bearings provide a remedy.