All messages - igus Blog - Page 67 All messages - igus Blog - Page 67

“We look forward to the next complaint”

igu-blog-adm | 15. February 2022

When I first heard this statement over 15 years ago, I thought, “We can’t be serious.” A complaint is a bad thing, it costs money, damages reputation, causes discord and involves a lot of work. Today, I stand rock solid behind that very statement. But why? The disappointed customer I would like to illustrate my […]

Read more...

Visualise condition monitoring system easily with the help of 3D data and schedule it at an early stage

Richard Habering | 7. February 2022

Condition monitoring systems are designed to eliminate unplanned downtime of machines and industrial plants by means of permanent condition monitoring. With the aid of 3D visualisations, these i.Sense systems can be integrated early in the design process.

Read more...

Four closed energy chains for dirt and chip protection that are guaranteed to work

jhang | 7. February 2022

In harsh environments, cables need to be protected from dust, chips, dirt and other external influences. The best protection is offered by the closed energy chains from igus® – also known as energy tubes or e-tubes. What are closed energy chains? Compared to open energy chains (picture 1), closed energy chains (diagram 2) are completely […]

Read more...

Conductor line retrofit with autoglide 5

Christian Strauch | 26. January 2022

Storage and retrieval units are often in use for more than 20 years. In the meantime, the units, like all machines, are regularly maintained, inspected, repaired and cleaned in a more or less fixed cycle whereby an electrical or mechanical retrofit is sometimes necessary. The conductor line in the aisle is an important part of […]

Read more...

Ball bearings for high-temperature applications – xirodur® A500

Patrick Czaja | 20. January 2022

With the market launch in 2007, igus achieved a milestone with the in-house material xirodur A500 for plastic ball bearings. This is because ball bearings made of this material have the specification of perfect functioning both at very high temperatures and in applications in chemical environments. Our ball bearings come without a drop of lubricating […]

Read more...