Many different shaft materials are used in the packaging, food and beverage industries. If a cost-effective solution is required, steel shafts are of interest. If light weight is important, aluminium shafts are used. If the application takes place in a humid environment or aggressive cleaning with chemicals, the corrosion resistance of the shaft is important. […]
I associate the topic of predictive maintenance with a reminder: just under two years ago, my wife gave me a great birthday present. A ride on a maize chopper. She had watched me playing the latest “agriculture simulator” weeks before and wanted to make me happy. (Did you know that the agriculture simulator is one […]
The use of strain relief components for energy supply systems is very often forgotten or simply underestimated and, when they are considered at all, they are often the wrong ones for the task at hand. This is extremely annoying and costs an unnecessary amount of time. But doing without strain relief is no solution either […]
Ball bearings consist of an inner and outer ring, a cage and rolling elements. The cage is used to separate the rolling elements from each other in the form of balls. If the balls were not separated, they would run against each other and overheat. With high rotational speeds and friction of the balls, destructive […]
In order to control the hoist on the indoor crane, a manual control unit, also known as a control device, is required. It can be moved along the crane girder independently of the hoist. This is to prevent people from standing below or in direct proximity to the lifted load when operating the indoor crane. With the guidefast control system there is also a suitable energy chain solution for such applications. The guidefast control system is installed directly on the crane girder and ensures a safe guidance of the control cable.