February, 2021 - igus Blog - Page 4 February, 2021 - igus Blog - Page 4

Polymer coating – the way to protect parts from wear and tear

Lars Butenschön | 5. February 2021

Surface coatings have long since established themselves in all areas of everyday life. From frying pans to bicycle frames, the range of different coating materials and their properties is huge. A more recent phenomenon is the so-called tribological polymer coating. These are plastic-based coatings that have been additionally improved tribologically – i.e. for use as […]

Read more...

How you benefit from igus’ global service

Volker Beissel | 5. February 2021

Globalisation as a buzzword is a broad term under which everyone imagines something different. At worst, you’re thinking of an Asian hotline for an American company. At best, you think of igus, with 35 branches and 4,150 contacts around the globe, for the best service. No matter where you build your machine or where you […]

Read more...

Lebensdauerrechner für 3D-gedruckte Bauteile

Unique service: determine service life of 3D printed polymer components

igu-blog-adm | 5. February 2021

Unplanned machine downtime is a horror for any engineer, especially as a failed component can, with a bit of bad luck, lead to serious damage of the machine. The associated costs and effort cause considerable trouble for many companies. Very few manufacturers are in a position to state the expected service life of their components. […]

Read more...

Thread size 10×3

Zoe Moser | 4. February 2021

The thread is a profiled indentation that runs along a helical line wound around a cylinder. The type of lead screw is defined by the profile shape, the pitch, the number of threads and the direction of rotation. You will find more terms related to lead screws in another blog post. Basically, lead screw drives are machine elements that convert rotary movement into linear motion. In this blog post we look at one of the common thread sizes: the 10×3 thread size.

Read more...

Kugellager in Pumpen

Ball bearings in pumps: prevent machine failures with polymer

Patrick Czaja | 4. February 2021

Pumps and compressors are used in a wide variety of industries. Whether, for example, hose pumps in medical and food technology or water pumps in pool technology: just as the heart is for humans, these types of pumps in industry are also to be regarded as the heart of the system.

Read more...