Shafts
If the metal ball bearing is a fixed or floating bearing, the outer and/or inner ring are firmly connected to the shaft or housing. The easiest way to mount this type of bearing is to press it into place. However, certain tolerances are necessary in the dimensions for the shaft and housing. In general, it […]
Self-aligning ball bearings (DIN 630) are double-row rolling bearings, consisting of an inner ring with a common ball raceway and an outer ring characterised by a hollow spherical design. Due to the hollow shape of the outer ring and the resulting angular mobility, self-aligning ball bearings are used in applications with larger misalignments, shaft deflections […]
The number of plain bearing solutions is virtually infinite, and there are no fewer designs of suitable – and unsuitable – shaft materials. In fact, different shaft materials and their coatings can create completely different wear patterns for the same plain bearing. This blog entry will deal with two frequently used shaft coatings and consider […]
Many different shaft materials are used in the packaging, food and beverage industries. If a cost-effective solution is required, steel shafts are of interest. If light weight is important, aluminium shafts are used. If the application takes place in a humid environment or aggressive cleaning with chemicals, the corrosion resistance of the shaft is important. […]
And again the working platform cracks, squeaks and crunches when the hydraulics are actuated. If noise is generated during operation or the device even jams, it is often already too late. Once you (or the appointed service technician) have located and dismantled the bearing, it often flashes and shines at you. Something like that! A […]