Plastic-ball-bearing
Many plant operators know the problem: when installing metal ball bearings, lubrication is essential. This procedure has to be repeated at regular maintenance intervals and that not only swallows up money, but also a lot of time. As a ball bearing alternative, xiros is well suited.
The defect of a ball bearing can have various causes; whether cage wear, ball breakage or damage to the running surfaces. Find out in this blog post why igus can be an alternative to metal after a defect.
Ball bearings cover a wide range of different shapes. Whether deep groove ball bearings, ball bearings with flange, for example, or self-aligning ball bearings: standard catalogues list these in various materials, designs and dimensions. But what about customised solutions? Customised ball bearings are no stranger to igus. xiros polymer ball bearings stand for quality. Due to […]
Manual sweepers are used both at home and in the industrial sector. Sweeping dirt and leaves on pavements or driveways with a leaf/sweeping broom is tedious, sweeping machines are a far better choice. In this case, the leaves and dirt are transported by brushes and a broom into a container, which can then be easily […]
Pools are everyone’s favourite; whether in summer for refreshment or in winter as an oasis of well-being at over 25°C in a Spa or Hot Tub. But here, too, there is a lot of technology backing it. The heart of every pool is the pool/water pump. Its purpose is to activate the water circulation in […]