Ball bearing - igus Blog Ball bearing - igus Blog

Keyword:

Ball bearing

New ball bearing material – ideal for applications in the semiconductor industry

Patrick Czaja | 19. May 2022

The semiconductor industry always has demanding application environments. For example, installed components must always run flawlessly in order to keep plant productivity rates high. The etching of printed circuit boards or the production of LCD displays are two examples to illustrate this.

Read more...

Kugellager-Alternative xiros aus Kunststoff von igus

Ball bearing alternative made of polymer: igus® convinces

Patrick Czaja | 16. February 2021

Many plant operators know the problem: when installing metal ball bearings, lubrication is essential. This procedure has to be repeated at regular maintenance intervals and that not only swallows up money, but also a lot of time. As a ball bearing alternative, xiros is well suited.

Read more...

When should I change my ball bearing?

Patrick Czaja | 11. February 2021

The defect of a ball bearing can have various causes; whether cage wear, ball breakage or damage to the running surfaces. Find out in this blog post why igus can be an alternative to metal after a defect.

Read more...

xiros Sonderteile für die Textilindustrie

Ball bearings according to specifications – an infinite number of possibilities thanks to igus®

Patrick Czaja | 9. February 2021

Ball bearings cover a wide range of different shapes. Whether deep groove ball bearings, ball bearings with flange, for example, or self-aligning ball bearings: standard catalogues list these in various materials, designs and dimensions. But what about customised solutions? Customised ball bearings are no stranger to igus. xiros polymer ball bearings stand for quality. Due to […]

Read more...

Ball bearings in manual sweepers: plastic defies dirt

Patrick Czaja | 2. February 2021

Manual sweepers are used both at home and in the industrial sector. Sweeping dirt and leaves on pavements or driveways with a leaf/sweeping broom is tedious, sweeping machines are a far better choice. In this case, the leaves and dirt are transported by brushes and a broom into a container, which can then be easily […]

Read more...