…also 1 kg with very high dynamics (see film). Result: a load to dead weight ratio of 1:1 becomes possible!
EvoLogics GmbH Vote Up +0 Vote Down -0You already voted!…
With CF.Q, CF.D and CF.P, igus has three sensors in the product range that are designed for chainflex cables.
CF.Q is the sensor for the…
…materials. Standard 3D printing materials behave differently, as they do not have an integrated lubrication. (see PA12 in graph).
Nevertheless, there are applications in which the components are smoothed…
Our customer PROFACTOR from Austria (https://www.profactor.at/) has shown a new low cost sorting solution at MOTEK show in Stuttgart. They use our robolink® joint arm RL-DQ-RBT-5532S for this task.
…
…the signals from the angle encoder are working. This is written in German.
http://www.mtahlers.de/index.php/grundlagen/robolink/encoder-as5304
http://www.mtahlers.de/index.php/grundlagen/robolink/quadratursignal
Thank you Malte!
Vote Up +0 Vote Down -0You already voted!…