The global circular economy is shrinking. It is high time to act. One solution would be to recycle technical plastics, but that has so far been quite cumbersome. We will show you how plastic recycling is finally becoming easy.
In today’s increasingly globalised world, service is often a nuisance for everyone. You have a problem with a household appliance, perhaps an oven, and you have specifically chosen a German brand. Luckily, the instructions also include a flyer with service numbers for each country. But when you enter the number into your phone, you always […]
One day after the trade show It happened near the beginning of the Hannover Messe, not all that long ago. They say that sometimes the best ideas come from a mix of nonsense and a little alcohol. Something like that must have been in play when the idea for the TRX emerged. Two exhausted, thirsty […]
Today I would like to introduce a topic that is often overlooked or not taken seriously, but can have a significant impact on the success of your business: professional energy chain installation. Whether you run a small manufacturing operation or manage a medium-sized facility, investing in the right expertise for your energy chain systems can […]
The use of strain relief components for energy supply systems is very often forgotten or simply underestimated and, when they are considered at all, they are often the wrong ones for the task at hand. This is extremely annoying and costs an unnecessary amount of time. But doing without strain relief is no solution either […]
Ball bearings consist of an inner and outer ring, a cage and rolling elements. The cage is used to separate the rolling elements from each other in the form of balls. If the balls were not separated, they would run against each other and overheat. With high rotational speeds and friction of the balls, destructive […]
In order to control the hoist on the indoor crane, a manual control unit, also known as a control device, is required. It can be moved along the crane girder independently of the hoist. This is to prevent people from standing below or in direct proximity to the lifted load when operating the indoor crane. With the guidefast control system there is also a suitable energy chain solution for such applications. The guidefast control system is installed directly on the crane girder and ensures a safe guidance of the control cable.
Machine tools have become an integral part of the industry. Thanks to them, metallic workpieces are produced with the highest precision, which are used, for example, in the automotive industry or in the aerospace industry. In all machine tools the desired contour is achieved by the interaction of tool and workpiece. Depending on the technology, […]