…in “English” (=germanenglish) and the second in german. please find some more written informations below.
http://blogtest.igus.com.br/int/wp-content/uploads/sites/2/2015/04/HMI2015_robolink_EN_01_1.mp4
in german:
I want to explain the basic idea of…
…bearings are advantageous because they are not only maintenance-free and lubricant-free, but also eliminate lubrication contamination on banknotes.
Glass balls provide an entirely metal-free variant, so our ball bearings…
…sensors detect condition and transmit real-time data to the user. This prevents expensive unplanned downtime. Read more about the use of igus smart plastics in the automotive area.
…Wago’s free app “WEBVISU”, that can be used on Apple and Android devices (mobile phone, iPad and so on). This is shown in the video attached:
http://blogtest.igus.com.br/int/wp-content/uploads/sites/2/2014/11/Robolink_IpadSteuerung.mp4
Vote…
…3,800m² test laboratory in Cologne. Here is a small overview of our test laboratory, which at that time was still somewhat smaller at 2,750m². Before bolting the robot to the…