All iglidur materials have advantages in this respect. They are insensitive to dirt, completely corrosion-free and do not need any lubrication. In many places where bearings are used in the agricultural area, large forces as well as impacts and shocks have an effect. Especially robust and durable iglidur materials such as iglidur G or iglidur M250 are particularly suitable […]
Reaming or increasing the hole size of iglidur plain bearings is possible without further ado, and can even have a positive effect on the running-in phase – the frictional properties when the component is in a new condition. Materials with a high fibre content, however, can become rougher or frayed during machining. You can find more […]
Reaming or increasing the hole size of iglidur plain bearings is possible without further ado, and can even have a positive effect on the running-in phase – the frictional properties when the component is in a new condition. Materials with a high fibre content, however, can become rougher or frayed during machining. Vote Up +0 Vote […]
In the case of plain bearings, the shaft moves permanently and is simultaneously in contact with the running surface of the bearing. This means that the nature of the shaft is as important for the service life of the system as that of the plain bearing. Whereas the properties of the plain bearing materials can […]
For uncomplicated and easy installation of our plain bearings, we recommend – a burr-free clean housing hole, ideally with slight chamfering – the hole tolerance H7 – ensuring that the plain bearing is not more than 2 % larger than the hole before it is press-fitted – installation by means of a flat press without […]