The linear carriages of TW series 01 always require a minimum amount of clearance between carriage and rail. They are delivered ready-to-install with preset clearance. Assembly The TW series 12 linear carriage must be pushed onto the hard-anodised TS-01 rail. The carriage is now ready to use. Clearance adjustment The bearing clearance can be adjusted […]
As an alternative to lubricated ball bushings, there is the clean, self-lubricating linear bearing adapter. The two cylindrical types have identical installation heights and can be installed in any linear housing. The two bearing types are also installed in the housing in exactly the same way. Firstly, a circlip is inserted into the inner groove […]
The automatic TWA linear carriages always require a minimum amount of clearance between carriage and rail. They are delivered ready to install with three adjusting keys. Assembly Insert all three keys into the carriage and “unlock” it by turning them anti-clockwise. Push the automatic TWA linear carriage onto the hard-anodised TS-01 rail. In the unloaded […]
The QWE linear carriages are delivered with a transport securing device, which simultaneously simplifies installation considerably. It is recommended that the securing device be retained for possible removal in future. Assembly The AWMQ hard-anodised, torque-resistant rail profile is pushed through the carriage. When this is done, the transport securing device is pushed out. (For removal, […]