iglidur - igus Blog iglidur - igus Blog

Tag: iglidur

Why wear-resistant 3D printing components made of iglidur plastics?

Dirk Zacharias | 1. August 2019

For manufacturing with 3D printers, you can choose from a wide range of technical plastics. Tribology know-how accumulated over decades is included in the development of our polymers. That way, you can find the iglidur high-performance plasticwith the perfect specifications for your application. For example for high loads, contact with food, media resistance or high […]

Read more...

How is the wear of iglidur iglidur plain bearings measured?

Lars Butenschön | 7. July 2019

The iglidur Expert system works on the basis of hundreds of thousands of measurements performed systematically in our tribo laboratory . Usually, in these tribological tests, wear-related material losses are determined by measuring the volume of wear and the weight loss of the bearing. In our experience, it is more practical to directly measure the […]

Read more...

How would I know when to change iglidur plain bearings?

Lars Butenschön | 7. July 2019

Most often, worn plain bearings are clearly noticeable. Unpleasant squeaks, rattling and clattering of the entire bearing or stiff movement are typical symptoms. If the bearing seizes, there is nothing one can do about it. The plant runs up against the block. It would be nice, of course, if you knew in advance when to […]

Read more...

Are there plain bearings that are resistant to mould?

Lars Butenschön | 7. July 2019

In technical building systems, vehicles and the aircraft industry, it occurs frequently: mould. This is not only annoying but is also a health threat that should be taken seriously. For this reason, the plain bearings used there must be resistant to fungi and bacteria. Therefore, we subjected our iglidur materials G, G1, J, H1, X, […]

Read more...

What is the difference between iglidur materials and simple plastics such as POM or PA6?

Lars Butenschön | 7. July 2019

iglidur materials are so-called compounds. Compounds are plastics to which special fillers, reinforcing agents and additives have been added. These give the plastic compound additional specifications such as higher mechanical stability, better sliding properties or protection against UV radiation. iglidur materials have been developed specifically for use as dry operating – i.e. without lubrication – […]

Read more...