Gliding application - igus Blog Gliding application - igus Blog

Tag: Gliding application

What should I consider for a side-mounted application?

Phillip Hagedorn | 7. July 2019

Especially when the installation space is tight, installing a side-mounted e-chain is helpful. It is important to pay attention to whether the e-chain glides on a surface or is designed for unsupported application. Gliding: If the e-chain is gliding horizontally mounted on the side, special attention must be paid to the following points: Use of […]

Read more...

Do energy chains influence the energy efficiency of the entire system over long paths?

Marco Thull | 5. July 2019

Energy chain systems not only transport energy, data and media to machinery and equipment. They also have an influence on their energy costs. How much pull and push force, in other words drive power, is required at a given speed to move an energy chain? How light but at the same time sturdy must energy […]

Read more...

What are the advantages and disadvantages of energy chains compared to motorised cable drums, festooning or busbar systems?

Marco Thull | 5. July 2019

What is decisive often is not the pros and cons of the individual systems but if the particular system is the right energy supply for my application in terms of cost, durability and installation space. For example, if you compare only motorised cable drums to energy chains, there is no blanket answer, because in the […]

Read more...

What should be considered in energy supply for use outdoors?

Marco Thull | 5. July 2019

Outdoor use is generally uncritical for energy supply systems. Energy chains are very tough and withstand extreme temperatures below freezing. Each energy chain is tested in the igus in-house test laboratory in a refrigerated container at -40 degrees Celsius and on an outdoor test track under real conditions. For special requirements, energy chains are also […]

Read more...

How often do you need to lubricate or replace the rollers on an energy chain system?

Marco Thull | 5. July 2019

The service life of the rollers of an energy supply system generally depends on the roller material and the external environment. Free-running or unprotected rollers are exposed to external influences. In energy chain systems, rollers are integrated in the chain link and “lubricated for life” with a seawater-resistant lubricant. A replacement for such a system […]

Read more...