The e-loop combines the advantages of a plastic e-chain with those of a high-tensile Dyneema rope. Ideal for three-dimensional movements. The tensile forces are absorbed by the rope and passed through the mounting brackets into the support structure. As a result, the cables are completely free of strain. The cable replacement is very simple: Unhook, […]
Almost every application for “long travels” has to be considered individually. As guidelines, a manual on this topic has been provided by igus for free as download . However, we recommend consulting with a service technician to select the right solution for your exact application. With more than 30,000 gliding applications, igus has the necessary […]
The upper run is the upper part of an energy chain. In a horizontal linear motion, the length of the upper run changes continuously. For this reason, the maximum unsupported upper run length must be taken into account in a horizontal application. This depends on the chain series, the additional load and the max. speed/acceleration. […]
The e-loopcombines the advantages of a plastic e-chain with those of a high-tensile Dyneema rope. Ideal for three-dimensional movements. The tensile forces are absorbed by the rope and passed through the mounting brackets into the support structure. As a result, the cables are completely free of strain. The maximum tensile force is 50 kN Vote […]
Energy chain systems not only transport energy, data and media to machinery and equipment. They also have an influence on their energy costs. How much pull and push force, in other words drive power, is required at a given speed to move an energy chain? How light but at the same time sturdy must energy […]