Are triflex R e-chains cleanroom compatible? - igus Blog Are triflex R e-chains cleanroom compatible? - igus Blog

Are triflex R e-chains cleanroom compatible?

cweiss | 5. July 2019

Are triflex R e-chains cleanroom compatible?

You are here:

triflex R e-chains can also be used in cleanroom applications. The used material igumid NB is used in other e-chains designs, which are certified with the ISO class 1 by the IPA Fraunhofer Institute. However, the application is decisive in 3-axis e-chains in robotic applications – in these applications, the energy supply often come into contact with the robot arm, causing abrasions from the resulting relative movements in the application. Although this can be reduced by the use of tribo-optimised materials and material combinations, it cannot be prevented 100% .

triflex r e-chains in a UR robot
You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

Cleanroom Industrial robots Robotics

Newsletter:

Choose a topic now