Plain Bearings - igus Blog - Page 26 Plain Bearings - igus Blog - Page 26

Category:

Plain Bearings

Spherical thrust bearing – 2 cost-effective alternatives

Lars Butenschön | 21. July 2020

The classic bearing position in the mechanical engineering textbook provides for a simple shaft in a ball or needle roller bearing that is mounted in a radial direction. But what if the bearing position must be supported axially? It is not uncommon for bolts or rods to be supported at the ends in an axial […]

Read more...

Designvorgang Buchse

Reduce costs for injection moulded parts – With these 3 tips

Lars Butenschön | 16. July 2020

The design rules for the most cost-effective injection moulding designs apply to plain bearings in particular, to wear-resistant parts in general and to all other components anyway. The pressure to save costs is particularly high for plain bearings and wear-resistant parts. As “disposable parts”, these should last as long as possible, but also cost as […]

Read more...

Lead screw technology in the DIY beer lift

Zoe Moser | 13. July 2020

A decisive point for the smooth application of the beer lift is the use of the correct high-helix thread system. The length of the lead screw is approx. 1 metre. In order to be able to guarantee the service life as long as possible, there are two important points to consider.

Read more...

xiros guide rollers with FDA conformity: 60% weight saving compared to metallic solutions

Patrick Czaja | 10. July 2020

This solution for transport and guide rollers is now available in a lighter, FDA-compliant version. The xiros guide rollers for labelling, packaging and food applications consist of a blue PVC tube and two fixed flange ball bearings made of the in-house material xirodur B180 and stainless steel balls. The specialist for plastics in motion, igus, […]

Read more...

What is iglidur? And what does it do better than POM?

Lars Butenschön | 2. July 2020

Just recently I stumbled on this blog post, which promised to finally put an end to the mystery that seems to be iglidur®. What is iglidur? And why are customers willing to spend no less than a fortune on bearings made from this material? To make this clear right away: I have no intention to […]

Read more...