Zoe Moser - igus Blog Zoe Moser - igus Blog

Knowledge of lead screw drive

Zoe Moser | 7. September 2022

Five things I should know about dryspin® lead screw technology: Importance of lead screw technology, details about the product range of dryspin® lead screw drives, difference in thread types, individual machining and configuration, and the lubrication of lead screw drives.

Read more...

Temperature lead screw nuts

Zoe Moser | 23. April 2021

Lead screw drives are used in many machines in a wide variety of industries. Thus, the demands placed on a lead screw drive also differ: from high and low loads to high and low speeds to large temperature spans or even permanent temperatures around 200°C. Of course, the screw drives used should also perform flawlessly here.

Read more...

Efficiency

Zoe Moser | 13. April 2021

In general, efficiency indicates how high the effectiveness of a device is when conversion losses are taken into account. The efficiency describes the relation between the delivered power (effective output) and the supplied power or loss and expenditure. In the calculation, the efficiency is abbreviated with a small eta (η). The result of the efficiency depends on what is considered a benefit or loss and what is considered an expenditure.

Read more...

Thread size 10×3

Zoe Moser | 4. February 2021

The thread is a profiled indentation that runs along a helical line wound around a cylinder. The type of lead screw is defined by the profile shape, the pitch, the number of threads and the direction of rotation. You will find more terms related to lead screws in another blog post. Basically, lead screw drives are machine elements that convert rotary movement into linear motion. In this blog post we look at one of the common thread sizes: the 10×3 thread size.

Read more...

Lead screw support

Zoe Moser | 4. December 2020

Our lead screw support blocks are available in thread sizes of 6 mm. Choice of mounting: plain bearings or, with higher dynamics, ball bearings (BB). All lead screw support blocks, like the matching lead screw clamp rings, are supplied in hard anodised aluminium.

Read more...