Patrick Czaja - igus Blog Patrick Czaja - igus Blog

Spring-loaded ball transfer units made of plastic for high shock loads

Patrick Czaja | 21. October 2022

Our ball transfer units can be used to move fragile or heavy goods easily and in all directions without much effort. We use various design concepts for this. In addition to injection-moulded housings with housing pads and ball beds, we also offer a variant with a sliding insert specially designed for higher loads and shock […]

Read more...

Some people rotate just so that everything revolves around them – xiros® uses a new material to enhance sustainability

Patrick Czaja | 14. October 2022

In keeping with our motto, "xiros® goes green", we are launching a ball bearing that contains 97% regranulate. We are moving in an environmentally friendly direction, since sustainability is becoming increasingly important, especially in industry. The reason is obvious, since industry is among the top three CO2 emitters worldwide.

Read more...

Ball bearings for electric motors – plastic versions feasible?

Patrick Czaja | 6. September 2022

Hardly any industry can do without electric motors in the entire value-added process and the demands placed on products are constantly increasing. Similarly, the requirements for the various components of the drives are also increasing in order to ensure smooth production processes, including for the bearing of components, namely ball bearings for electric motors. But […]

Read more...

Which ball bearing is suitable for high speeds?

Patrick Czaja | 2. June 2022

Deep groove ball bearings according to DIN 625 standard are the most commonly used ball bearings in industry. Depending on the application, plant operators have different requirements for the installed machine components. For deep groove ball bearings, for example, the possible speeds per minute are usually important. Which ball bearing is suitable for high speeds? And that even made of plastic? xiros is the answer.

Read more...

New ball bearing material – ideal for applications in the semiconductor industry

Patrick Czaja | 19. May 2022

The semiconductor industry always has demanding application environments. For example, installed components must always run flawlessly in order to keep plant productivity rates high. The etching of printed circuit boards or the production of LCD displays are two examples to illustrate this.

Read more...