And again the working platform cracks, squeaks and crunches when the hydraulics are actuated. If noise is generated during operation or the device even jams, it is often already too late. Once you (or the appointed service technician) have located and dismantled the bearing, it often flashes and shines at you. Something like that! A […]
Bearings for EX and ATEX – A small guideline Trying to search for bearings suitable for environments with explosive atmospheres online is not easy. In fact, you will end up with more questions than answers. Which materials are suitable? What exactly is ATEX and what does it require? And what about plastic bearings? Aren’t they […]
It´s common knowledge, that together with duct tape, WD-40 is THE universal tool to fix anything and everything. While the former keeps everything in place when it shouldn´t be moving, the latter keeps things going that shouldn´t stand still. Many people think that these two tools will set you up for almost anything life throws […]
At first glance, many advantages of plain bearings sound attractive for use as roller. They use less space than roller bearings, require no additional lubrication (depending on their type) and do not suffer as much from dirt and cleaning agents. On top of that they weigh less and are cheaper. But as usual, devil is […]
The various influences that affect the lifespan of a plain bearing are relatively trivial. It´s easy to imagine that a truckload of fine dust is rather less helpful for a long bearing life. Also, that 500 ° C ambient temperature can cause difficulty in choosing the right lubricant, results in few raised eyebrows. And yet, often times […]