Jens Göbel - igus Blog - Page 2 Jens Göbel - igus Blog - Page 2

Zig-zag on the indoor crane – the unusual cable guidance for lifting applications

Jens Göbel | 24. April 2020

For many lifting applications, a compact, space-saving solution is extremely important. But the more cables coming together in a system and the higher the stroke, the fewer the plausible solutions. If the liftband or the e-spool reaches its limits, the zig-zag installation is often the only thing that remains.

Read more...

e-spool – the alternative to the cable drum on an indoor crane

Jens Göbel | 21. April 2020

The e-spool is a chain-based drum application without sliding contacts. Ideal for applications and load-carrying equipment constructions that have no room for a collection basket (lift strap). The cables guided in the chain are not exposed to tensile strain, which has a positive effect on the service life of the cables.

Read more...

Energy chains on indoor cranes under rough conditions – how resilient are polymer chains?

Jens Göbel | 18. April 2020

As versatile as the various indoor crane designs are, their areas of application are just as varied. The advantages of the energy chain over other cable or power supply systems are particularly evident under adverse operating conditions. Suitable for both trolley drive and crane drive, heavy-duty energy chains, with and without integrated skate wheels, can master even the most difficult operating conditions.

Read more...

Relevant regulations for vending machine manufacturers in the food sector

Jens Göbel | 17. April 2020

There are a number of standards for vending machine manufacturers in the food sector. Here is

Read more...

Safe control device guide on indoor crane

Jens Göbel | 14. April 2020

In order to control the hoist on the indoor crane, a manual control unit, also known as a control device, is required. It can be moved along the crane girder independently of the hoist. This is to prevent people from standing below or in direct proximity to the lifted load when operating the indoor crane. With the guidefast control system there is also a suitable energy chain solution for such applications. The guidefast control system is installed directly on the crane girder and ensures a safe guidance of the control cable.

Read more...