All messages - igus Blog - Page 91 All messages - igus Blog - Page 91

Hard on the outside, smart on the inside: intelligent plain bearings enable continuous condition monitoring

Richard Habering | 7. April 2021

Plain bearings often have to withstand considerable adverse influences such as abrasive dust, high speeds or chemicals. To enable indication of the degree of wear of such plain bearings in good time, last year igus developed the world’s first intelligent bearing with iglidur high-performance polymers. This warns of imminent failure in good time. Machine and equipment operators can plan maintenance, repairs and part replacement in advance.

Read more...

How to connect igus® encoders with Beckhoff and B&R

Adriana Glazer | 7. April 2021

There are control systems whose encoder card is usually compatible with 24V and/or single-ended encoders. igus motors, however, work with 5V and as line drivers. A connection of these two voltages requires another component or a special encoder card.Today we are looking at the connection of igus motors to control systems that work with 24V […]

Read more...

Condition monitoring is synonymous with i.Sense at igus

Richard Habering | 31. March 2021

In this particular case, I will focus on the concept of condition monitoring. This technology at igus is called i.Sense and is derived from sensing/feeling. We found the name quite appropriate, as condition monitoring has exactly this function: the sensing of malfunctions.

Read more...

Condition monitoring of linear robots

Richard Habering | 26. March 2021

This or something similar must have happened between Güdel and igus at one of the earlier Hannover Messe events. It was decided, probably along with a handshake, to feed the condition monitoring system from Güdel with the data from the condition monitoring system from igus (i.Sense).

Read more...

You don’t play with water! Or do you?

Patrick Czaja | 25. March 2021

Warm summer evenings, starry skies and marvelling at a choreography with colourful water fountains and walls supported by music – a great feeling. However, there is quite a bit of technology behind this breathtaking light and water show. If there is a technical error or even a defect in the components, the choreography can quickly […]

Read more...