Die Diskussion über die weltweit durch Kraftfahrzeuge erzeugte CO2-Emission stellt eine Herausforderung für jeden Entwickler in der Automobilindustrie dar. Neben der Optimierung des Motors, des Antriebstrangs und weiteren Komponenten spielt die Reduzierung von Gewicht eine wichtige Rolle, um den Schadstoffausstoß zu minimieren. Bei Verbrennungsmotoren, wie auch in der Elektromobilität, hat die Wahl der eingesetzten Materialien […]
What specific advantages does the energy chain have over the classical festooning or cable trolley system in an indoor crane? Increased interior range without obstacles. Unexcelled distances under the entire crane girder. Low chain system installation space necessary on the crane. No cables dangling from the crane girder – greater storage space. Small clearance between the hook and the wall. Longer cable service life. Operating and maintenance costs lower than those of festooning or a cable trolley system. Less susceptibility to errors. No components that require regular lubrication.
Harnessed energy chains in automatic medication picking systems face special requirements.
Electrical engineering is often concerned with motor cables as well as servo cables. But what is exactly the difference between a servo cable and a motor cable? And can I use a servo cable to connect a normal three-phase motor? What exactly are the differences? The fact is that both cables are designed to supply […]
Medical technology is an important driver of 3D printing technologies: highly customisable products offer unprecedented opportunities for a wide range of medical solutions. Components from 3D printers are used in the production of individually manufactured components for patients, such as hearing aids. Hospitals are acquiring their own 3D printers so that they can quickly create […]