The material for rolling bearing ball bearing balls varies widely and is always primarily focused on the ring materials. This ensures that the interplay of cage, inner ring, and outer ring in the system is harmonised. This is especially important when the application involves heating or cooling the bearings. It is important that ball bearing […]
The decisive factors in today’s plastic processing industry are efficiency and productivity. That is why automation processes such as machine feeding, component handling and pick-and-place processes are essential components of modern, economic production. Automation made easy with igus Low Cost Automation.
For pivoting and rotary movements of up to 270°, it is important that cables and hoses are laid in the energy chain’s neutral phase. Why is this so important? Pivoting and rotary movements usually involve winding up the e-chain or guiding it into an S shape. For normal installation positions (horizontal, standing, or suspended), the […]
The cable guide problem can be solved with an energy chain on indoor cranes with two trolleys as well. But two trolleys must not always be the reason for a reverse energy chain application.
A tooth breaks on a gear, and that’s all it takes to stop the machine. Unfortunately, the documentation has been lost, and the manufacturer does not supply spare parts any more and may even have gone out of business. What now? The gear must be replaced, and there are no clues besides the broken component. […]