Most plain bearing manufacturers – and igus® is no exception – advertise their bearings with the attribute “insensitive to dirt”. But what does that actually mean? And what do you do when you have exhausted the limits of this rather subjectively formulated concept? In equipment intended for really rough environments, such as mining, earthworks on […]
There are many different possibilities to synchronise several adjustments in one system. But which is the right one for me and my application? Often not easy to answer. But what if it should be simple and uncomplicated? What are the options? The market offers different solutions for different applications. The most commonly used system is […]
Maintenance is a central point when operating machines. On the one hand, this ensures operational safety. On the other hand, maintenance is associated with expenditure. This expenditure is divided up as follows: The machine is at a standstill during maintenance. Depending on the machine, this is expensive. A construction machine cannot be rented. And problematic […]
igus has the world’s largest test laboratory for plastics in moving applications in Cologne, with around 12,000 tests per year. This includes tests that demand everything from the most diverse materials under the most adverse conditions. At the present test, a xiros fixed flange ball bearing competes against its metallic counterpart in a salt water […]
Injection moulding is one of the primary processing methods in plastics processing. It is the most widely used processing method. About one third of all plastics are processed on injection moulding machines. Energy chain systems, highly flexible cables and bearing technology solutions by igus ensure a long service life of all parts of injection moulding machines.