Installation situation e-chain with moving lower run Sometimes the installation situation requires turning the orientation of the e-chain and turning it upside down, so to speak. The fixed end is mounted “up” and the moving end is “down”. This is a very special installation situation and places other demands on the design of the energy […]
In the water bath the extrudate is guided by rollers and kept at a distance. The rollers run with pressed-in stainless steel ball bearings without seals. These run completely under water. Despite the stainless steel design, these had to be replaced at regular intervals due to corrosion. igus polymer ball bearings provide a remedy.
Large bearing diameters tailor-made at an off-the-shelf price! The largest selection of different dimensions is offered by “the generalist” iglidur G. The smallest bearing has an inner diameter of 3mm (smaller inner diameters are available for other iglidur materials). The largest inner diameter of an igus catalogue part is 195mm. Part No.: GFM-195205240-65 (Outer diameter […]
Cables have to withstand the most diverse external conditions today. This depends entirely on the areas and applications in which they are used. Today we take a look at what you have to pay attention to with cables in cold applications. What does temperature-resistant mean? Cables fit for use in extreme temperature ranges are referred […]
People often look for ways to reduce the cost of a machine tool. Of course there should be no loss of service life. The large chains of the X, Y and Z axes were then already discussed in detail with a colleague and the most favourable solution that works was selected. But there is also […]