At first sight the process of soldering looks simple, but on closer inspection it is a complicated process that needs to be mastered. The freely manually tin-plated contact is very much dependent on the person carrying out the work as well as on the temperature, the solder used and the size of the components to be connected and is subject to certain fluctuations. Correct soldering must therefore be learned. If you observe a few criteria and with a little practice, soldering is no problem.
Anyone who has ever wanted to order an igus linear axis is inevitably asked at some point what orientation the motor should have. Left, centre, right, 0° or 90°? It all sounds like choosing your party before the local elections, but it is much easier than that. What is meant by motor alignment? By motor […]
Winding data cables and media hoses on cable drums? Because this does not work without complex and expensive slip ring technology, cables lying on the floor become a fall hazard in many companies. The alternative: the e-spool-flex cable drum with uninterrupted screw guide. Monday morning in an industrial hall: a technician wants to configure a […]
Why the issue of linear rail length? Does it matter, because it depends on every application and installation location? Yes, exactly right… The length is always different and individual. No two applications are the same. Suppose we build a piece of furniture and are looking for a linear guide. The available space inside the table […]
The dryspin lead screw technology was developed and patented in 2016 by the drylin lead screw technology development team. Particular emphasis was placed on increasing service life and improving efficiency. The dryspin product portfolio includes high-helix lead screws made of stainless steel or aluminium and the matching lead screw nuts made of igus high-performance polymers.