What do I do if the unsupported length is exceeded?
If the unsupported length of a series is exceeded according to the FLG diagram (fill weight, travel), the following options are available.
- Choose a more stable e-chain.
Example: E4.42, additional weight 15 kg/m; travel/unsupported length: 5 m/2.5 m

Under these conditions, the E4.42 is in “critical sag”. If an energy chain is required in the unsupported area with straight upper run, the series 15050/15150, for example, can be used.
2. The e-chain can be supported in the unsupported area. However, this is associated with limitations in acceleration, speed and noise generation.

3. A multiband e-chain®/extension link can be used to increase the load capacity.

4. The travel can be designed as a gliding application.