You have certainly heard of it – the new SEW-Eurodrive: Movilink® DDI generation of drives. They are drive motors with a digital data interface. The supply cable is a hybrid cable with a coaxial element. So far, so good! But of course you would also like to have this engine generation in SRUs, cross-traversing trolleys, […]
Nowadays, it is all about avoiding waste. The oceans are heavily polluted, the “Pacific garbage vortex” is about 4.5 times as large as Germany. The “zero waste” philosophy is gaining more and more attention especially in the food sector. We at igus have also set ourselves the goal of buildings and production becoming CO2-neutral by […]
Deep groove ball bearings according to DIN 625 standard are the most commonly used ball bearings in industry. Depending on the application, plant operators have different requirements for the installed machine components. For deep groove ball bearings, for example, the possible speeds per minute are usually important. Which ball bearing is suitable for high speeds? And that even made of plastic? xiros is the answer.